Anchoring Conditions – Edge Distance, Embedment & Installation Requirements
The performance of an anchoring system depends on more than the anchor itself. Edge distance, anchor spacing, embedment depth, base-material condition and installation quality all influence how loads are transferred into the surrounding material.
For structural applications, these conditions should be considered together during anchor selection and design. The requirements for a specific anchor are defined by its technical documentation, relevant European Technical Assessment (ETA) and the applicable design method.
Why anchoring conditions matter
An anchor that performs well under one set of conditions may have a different resistance when installed close to an edge, near another anchor or with a reduced embedment depth.
Important design and installation conditions include:
- Edge distance
- Spacing between anchors
- Effective embedment depth
- Drill-hole depth and diameter
- Concrete-member thickness
- Fixture or clamping thickness
- Drill-hole cleaning
- Cracked or non-cracked concrete
- Installation temperature
- Environmental exposure
- Fire or seismic requirements where applicable
Do not consider these parameters independently. Changing one condition can influence the resistance or suitability of the complete anchorage.
Edge distance and anchor spacing
An anchor's position within the base material can significantly affect its performance.
An anchor installed close to the edge of a concrete member may have less surrounding concrete available to resist the applied load. Similarly, anchors positioned close together can influence the same area of concrete and may interact with one another.
Edge distance
Edge distance is the distance between the centreline of an anchor and the edge of the concrete member. Reduced edge distances can influence resistance, particularly where tension or shear forces create stresses in the surrounding concrete.
The permissible edge distance depends on the anchor system, loading direction, concrete condition, embedment depth and applicable product assessment.
Anchor spacing
Anchor spacing is the distance between neighbouring anchors. When anchors are installed sufficiently far apart, each anchorage may behave largely independently. At reduced spacing, their load-transfer zones can overlap, and the anchor group's resistance may be affected.
Therefore, no single universal minimum spacing or edge distance applies to all anchoring systems. Take the relevant values from the product documentation and consider them in the structural design.
Learn how spacing and edge distance affect anchor loads >
Embedment depth and drill-hole depth
Embedment depth describes how far the load-transferring part of an anchor extends into the base material. It is one of the important parameters influencing anchor resistance.
Greater embedment can increase the amount of base material involved in transferring the load, but suitable embedment depths depend on the anchor system and application.
Effective embedment depth
Effective embedment depth It should not automatically be assumed to be the same as the overall anchor length or the total depth of the drilled hole.
Drill-hole depth
The drill hole may need to extend beyond the effective embedment depth to accommodate the anchor, drilling dust or the installation method. Always follow the manufacturer's installation instructions for required hole depth and diameter.
Drilling deeper or shallower than specified can affect installation quality and anchor performance.
Installation conditions at a glance
Geometry
Edge distance, anchor spacing, embedment depth, member thickness and fixture dimensions all influence the geometry of the anchorage.
Installation
Correct drilling, hole cleaning, installation depth, tightening, and curing (where applicable) are essential to achieving the intended anchor performance.
Environment
Moisture, temperature, corrosion exposure, fire requirements and other service conditions can influence anchor selection and material choice.
Drill-hole cleaning
Correct drill-hole preparation is an important part of anchor installation. Dust and drilling debris can interfere with the way an anchor transfers load into the base material.
This is particularly important for bonded and chemical anchoring systems, where the bonding material needs effective contact with the wall of the drilled hole.

Depending on the anchor system, the specified cleaning procedure may include blowing, brushing, vacuum cleaning or a defined combination of these steps.
The required method, equipment and number of cleaning operations should always follow the installation instructions for the specific anchoring system rather than relying on a generic cleaning sequence.
Correct drilling is essential
Drill-hole diameter, drilling method and hole depth can all influence anchor installation.
Use the specified drill bit diameter, and form the hole using the drilling method stated in the relevant product documentation. Different base materials or anchoring systems may require different drilling techniques.
Excessively worn or unsuitable drill bits can create holes outside the intended dimensions and may affect anchor performance.
Fixture and clamping thickness
The thickness of the component being fixed influences the required anchor length and the anchor's position within the base material.
When determining the appropriate anchor size, the complete fixing arrangement may need to account for:
- Fixture thickness
- Washers and other components
- Levelling or packing materials
- Required embedment depth
- Thread engagement or tightening requirements
An anchor should provide the required embedment while also accommodating the complete fixture thickness within its approved installation range.
Concrete thickness
The thickness of the concrete member is another important anchoring condition. Sufficient base material must be present below and around the anchor to accommodate the required embedment and allow loads to be transferred safely.
Installing an anchor in a concrete member that is too thin can influence resistance and may increase the risk of concrete splitting or damage during drilling and installation.
Therefore, check the minimum member thickness against the requirements for the specific anchor system.
Cracked and non-cracked concrete
Concrete condition also affects anchor design. Anchors installed in areas where cracks can develop need to be suitable for cracked concrete where required by the application.
The selected anchor and calculation should reflect whether the concrete can be considered non-cracked or whether cracked concrete must be assumed.
Learn more about cracked and non-cracked concrete >
Temperature and installation conditions
Temperature can influence both installation and in-service performance, particularly for bonded anchoring systems.
For chemical anchors, the base material temperature can affect curing time. Installation procedures may therefore specify different curing periods depending on the temperature at the time of installation.
Check the permitted installation temperature and service-temperature range in the relevant product documentation.
Do not load an anchor until the required installation or curing conditions have been achieved.
Corrosion and environmental exposure
Consider the environment in which an anchor is installed when selecting its material and corrosion protection.
Exposure conditions can range from dry indoor environments to external, humid or chemically aggressive locations.
Factors to consider include:
- Indoor or outdoor use
- Humidity and condensation
- Direct exposure to weather
- Industrial or chemical environments
- Marine or chloride exposure
- Expected service life
- Compatibility with the fixture and surrounding materials
The anchor material or protective finish should suit the relevant environmental conditions and the application requirements.
Fire resistance
Where an anchorage forms part of a structure or system that is required to perform during fire, the anchor must be suitable for the relevant fire conditions.
Elevated temperatures can reduce the strength of both the anchor and the surrounding concrete. Therefore, fire resistance should be assessed using product-specific performance data and the applicable design requirements.
Fire performance should not be assumed simply because an anchor is approved for normal structural use.
Seismic conditions
Seismic loading can place additional demands on an anchoring system through movement, cracking and cyclic loading of the concrete.
Where seismic design is required, the selected anchor must have the appropriate assessment for the intended seismic application and the anchorage should be calculated using the applicable design conditions.
Approval for cracked concrete does not automatically mean that an anchor is suitable for seismic applications.
How anchoring conditions affect load capacity
Anchor resistance cannot be determined from the anchor diameter or material alone. The surrounding geometry and installation conditions form part of the overall anchoring system.
Reduced edge distances, restricted spacing, limited embedment depth or insufficient concrete thickness can all affect the available resistance.
The direction and magnitude of the applied loads must therefore be assessed together with these installation conditions.
Explore tension, shear and combined anchor loads >
Calculate edge distances, spacing and embedment
For structural fastenings in concrete, the relationship between applied loads and installation geometry can become complex, particularly where several anchors form part of the same connection.
The Fabory Anchor Calculator helps you design post-installed anchors for structural use in concrete in accordance with EN 1992-4.
Use the calculator to assess:
- Anchor position and configuration
- Edge distances
- Spacing between anchors
- Embedment conditions
- Tension and shear loads
- Combined loading
- Cracked and non-cracked concrete
- Fire and seismic conditions where applicable
The calculator checks the anchors in the available catalogue against the entered design parameters and identifies solutions that meet the relevant structural requirements.
Use the Fabory Anchor Calculator >
EN 1992-4 and anchor approvals
For post-installed structural fastenings in concrete in Europe, EN 1992-4 provides the design framework used together with the product-specific performance information for the selected anchor.
The relevant European Technical Assessment (ETA) defines important conditions for the individual anchoring system, which can include:
- Approved base materials and concrete strength classes
- Cracked or non-cracked concrete
- Anchor dimensions and embedment depths
- Minimum spacing and edge distances
- Minimum concrete-member thickness
- Installation procedures
- Loading conditions
- Environmental or service conditions
Structural anchor design should therefore use the parameters applicable to the specific product rather than generic spacing, edge-distance or installation values.
Explore more anchoring guidance
Continue exploring Fabory's technical anchoring guidance:
- Types of anchors >
- Understanding anchor loads >
- Anchoring base materials >
- Cracked and non-cracked concrete >
- Practical anchor design >
- Explore all anchoring technical guidance >
Need help with an anchoring application?
Anchor geometry and installation conditions can become complex where multiple anchors, restricted edge distances, high loads or additional fire or seismic requirements are involved.
Fabory's technical specialists can help you assess the application requirements and identify a suitable anchoring solution.
Contact our technical specialists >
Frequently asked questions about anchoring conditions
Find answers to common questions about edge distance, anchor spacing, embedment depth and installation requirements.
What is edge distance when installing an anchor?
Edge distance is the distance between the centreline of an anchor and the edge of the base material. Reduced edge distance can affect anchorage resistance because less surrounding concrete is available to transfer the applied loads.
How far apart should concrete anchors be?
No single spacing applies to every concrete anchor. Required and minimum anchor spacing depend on the anchoring system, embedment depth, loading conditions, concrete condition and product approval. Check the values for the specific anchor in its technical documentation and consider them in the structural calculation.
What is effective embedment depth?
Effective embedment depth is the depth over which an anchor transfers load into the surrounding base material. It is an important design parameter and should not automatically be assumed to be the same as the overall anchor length or drilled-hole depth.
Why is drill-hole cleaning important for chemical anchors?
Dust and drilling debris can interfere with the bond between a chemical anchoring system and the wall of the drill hole. The hole should therefore be cleaned using the procedure specified for the particular anchoring system before installing the bonding material and anchor element.
Do edge distance and anchor spacing affect load capacity?
Yes. Anchors installed close to an edge or close to one another can have lower resistance than anchors installed with unrestricted spacing and edge distance. The effect depends on the anchor system, geometry, concrete condition and loading direction.
Can the Fabory Anchor Calculator check edge distances and anchor spacing?
Yes. The Fabory Anchor Calculator allows the anchoring geometry and applied loads to be entered so that suitable post-installed anchors for structural use in concrete can be assessed in accordance with EN 1992-4.