text.skipToContent text.skipToNavigation

WAŻNE! W wyniku awarii poczty mailowej nie dotarły do nas wiadomości wysłane 13.11. Prosimy o ich ponowne przesłanie. Przepraszamy za utrudnienia!

Anchor calculation software interface for structural fixings in concrete

Documentation is part of getting steel construction right

In steel construction, product selection is only part of the wider requirement. Documentation, certificates and traceability also play a critical role in supporting compliance, project control and final handover.

Whether the project involves structural bolting, anchoring systems, threaded rods or other approved components, buyers and technical teams often need more than a product code. They need the right documents to show what has been supplied, what standard applies and how the product supports the project requirement.

For engineers, procurement teams and QA professionals, understanding which documents matter helps reduce risk and supports smoother project execution from specification through to handover.

Good documentation reduces uncertainty across the project

In steel construction, missing documents can create just as much friction as the wrong product choice. Delays in procurement, uncertainty during quality checks and incomplete handover files can all slow a project down and create unnecessary risk.

Certificates and supporting documents matter because they help connect the supplied product to the required standard, declared performance or traceability route. That can be critical for technical review, site acceptance, audits and customer confidence.

In practice, strong documentation helps teams make faster, more confident decisions and maintain better control over compliance throughout the project lifecycle.

What documentation typically means in this context

In steel construction, documentation can include certificates, declarations, technical files, product data and traceability records that support product selection and project compliance.

The exact documents needed will depend on the product type, the standard involved and the project requirement. Some documents help confirm material or batch traceability, while others relate to declared performance, technical assessment or conformity to a structural standard.

The main document types teams often check

The right document depends on the product and project requirement, but the most common need is to show compliance, performance or traceability clearly.

In many steel construction projects, the document check is not about collecting paperwork for its own sake. It is about making sure the supplied product is supported by the right evidence for specification, quality review and final project records.

• test certificates
• declarations of performance
• ETA-related documents for approved systems
• product data sheets and technical information
• traceability and batch-related supporting records

What test certificates help support

Test certificates are often used where material or batch-related confirmation is needed as part of the supply and traceability process.

Test certificates can play an important role where projects require visibility of product or material-related information linked to supply. They are often relevant in applications where traceability, verification or supporting technical records matter to the customer or project file.

The exact certificate type required should always be checked against the project specification. What matters most is ensuring the requested document is appropriate to the product and the compliance route being followed.

What DoP and ETA-related documents help support

DoP and ETA-related documents are often used where the project needs visibility of declared performance or approved application scope.

For anchoring systems and other approved construction products, documents linked to Declaration of Performance and European Technical Assessment can be central to product review. They help teams understand the declared performance route and the technical basis behind intended use.

These documents are especially relevant where engineers, QA teams and procurement functions need stronger confidence that the selected product aligns with specification and project documentation requirements.

Documentation and traceability are related, but not the same

A common mistake is to assume that any certificate automatically covers the full traceability or compliance requirement for the product.

Documentation = the supporting records linked to product selection and compliance

Traceability = the ability to connect the supplied product back to a defined source or record

The simplest way to understand the difference is this: documentation refers to the wider set of records that support compliance and project control, while traceability refers more specifically to the ability to link the supplied product to a defined batch, source or supporting record.

Both matter in steel construction, but they solve different problems. One supports confidence in what the product is and how it aligns with the project requirement. The other supports confidence in where it came from and how it can be verified.

Documentation in steel construction at a glance

Topic Main role Why it matters
Test certificates Support material or supply-related verification Useful for traceability and project records
DoP Declares product performance Supports compliance review and project documentation
ETA-related documents Support technical assessment and intended use Helps teams review suitability and scope
Product data and technical sheets Provide product information and application guidance Useful for selection and technical reference
Traceability records Link supplied goods to a defined source or batch Supports audit readiness and verification

When documentation should be checked

Documentation should be reviewed before supply becomes urgent, not after the product is already on site.

The best time to confirm certificate and documentation needs is before ordering, while the product route and project requirement are still being reviewed.

Checking documentation early helps avoid last-minute problems. It gives teams time to confirm what is needed for specification, procurement, site acceptance and final handover without creating delay later in the process.

Documentation review is especially useful:
• during specification and product selection
• before ordering approved or structural products
• when QA teams are defining project file requirements
• before handover documentation is compiled

What buyers, engineers and QA teams should check

Before ordering steel construction products, it is worth checking the standard, document route, traceability requirement, product match and project file needs.

Strong documentation control starts before purchase, not after delivery.

1

What does the project specification require?

The required document set should come from the project need, not from assumptions about what is usually supplied.

2

Which document type is actually needed?

Teams should confirm whether they need a test certificate, DoP, ETA-related document, data sheet or traceability support.

3

Does the documentation match the product being supplied?

Generic or unrelated paperwork can create confusion later if it does not clearly align with the selected product.

4

Is traceability part of the requirement?

In some projects, the ability to link the supplied product to a batch or source record is just as important as the document itself.

5

What needs to go into the final project file?

QA and handover teams should know early what needs to be retained for audits, records and final submission.

Common mistakes to avoid

Documentation problems usually start when teams treat all certificates as interchangeable or leave the check too late in the process.

Assuming one document covers everything

Different documents support different parts of the compliance and traceability requirement. One file rarely answers every need.

Waiting until delivery to confirm paperwork

By that stage, any missing or incorrect document can create unnecessary delay for procurement, QA or site teams.

Using documents that do not clearly match the supplied product

Paperwork is only useful when it can be connected clearly to the selected product and its intended compliance route.

Overlooking handover requirements

Missing records often become a problem at the end of the project when teams need to complete the final documentation pack.

How Fabory supports documentation readiness

The right support is not only about supplying product. It is also about helping teams manage the wider documentation requirement with more confidence.

Fabory helps customers reduce uncertainty around certificates, documentation routes and steel construction product support.

Fabory supports customers with more than product availability alone. The wider approach is built around helping engineers, procurement teams and QA functions make more confident product decisions while keeping documentation and project readiness in view.

Fabory support can include:
• support for product selection aligned to project needs
• guidance around documentation availability
• support for engineers, buyers and QA teams
• availability and continuity of supply
• a stronger route to project documentation readiness

The aim is to help customers reduce uncertainty around both the product route and the supporting records needed across the project lifecycle.

Related topics worth exploring

Documentation in steel construction often sits alongside wider questions about standards, approved products and project compliance.

ETA and DoP explained for anchoring systems
Anchoring steel to concrete
EN 15048 vs EN 14399
Threaded rods and studs in steel construction
Mechanical and chemical anchor selection

Need support with certificates and documentation in steel construction?

Talk to Fabory about steel construction products, documentation support and the right route for compliant selection and supply.

Talk to Fabory
Nie zamykaj tej strony. Ten komunikat zniknie, gdy strona zostanie w pełni załadowana.