Knowledge hub
Choosing screws for plastic housings in electrical appliances
The screws in a plastic appliance housing hold covers, panels and internal parts in place through years of heat, vibration and servicing. The wrong screw can crack the boss, strip the thread on the line or loosen in service. Choosing well comes down to four things: the right screw type, the right hole size, a well-designed boss and a controlled assembly process.

In this article
01
Match the screw to the plastic
Thread-forming screws for thermoplastics, thread-cutting screws for thermosets. Keep standard sheet-metal screws out of plastic bosses.
02
Size the hole correctly
Most thermoplastics need a pilot hole of 0.70 to 0.85 times the screw diameter. Use the screw maker's data for your material.
03
Control torque and speed
Set torque between driving and stripping torque, and drive at moderate speed so the plastic does not melt.
Why plastic joints need different thinking
In metal, a screw only has to clamp. In plastic, it also has to form its own thread in a material that is weaker, softer and more sensitive to stress than steel. Too much outward force cracks the boss; too much torque strips the thread.
The plastic decides which screw works. As a typical guide, thread-forming screws suit thermoplastics with a flexural modulus of roughly 1,000 to 2,800 MPa, while thread-cutting screws suit stiffer, more brittle thermosets of roughly 3,400 to 14,000 MPa. White goods are among the biggest users of thread-forming screws.
There is no single standard for screws in plastic, so screw makers publish design data for each thread form. This covers the hole diameter for each plastic, the boss outer diameter and thread engagement depth, and the drive and stripping torque to expect.
Always design to the data for the screw you are using, and confirm the final design by testing in your actual material and mould.
Choosing the screw type
Best for thermoplastics
Thread-forming screw for plastics
- Strengths
- Displaces plastic without chips, high pull-out strength and low stress on the boss.
- Watch out for
- Hole size and torque must suit the material.
- Typical use
- Housings and covers in ABS, PC, PP, PA, PBT and blends.
For thermosets
Thread-cutting screw
- Strengths
- Cuts a clean thread in brittle material.
- Watch out for
- Weaker hold in ductile thermoplastics, and chips must clear the hole.
- Typical use
- Thermosets and other brittle plastics.
For repeated opening
Threaded insert with machine screw
- Strengths
- A metal thread that survives repeated assembly.
- Watch out for
- An extra part and process step.
- Typical use
- Panels and covers opened often in service.
Avoid in plastic bosses
Standard self-tapping screw
- Strengths
- Low cost and widely available.
- Watch out for
- The coarse 60° sheet-metal thread puts high radial stress on the boss and can crack it.
- Typical use
- Thin sheet metal, not plastic bosses.
A screw for plastics has a narrower thread flank than a standard screw, typically 30° or less instead of 60°. That pushes the plastic along the screw rather than outwards, reducing the bursting force on the boss. Wider thread spacing also leaves more plastic between the threads, which improves pull-out strength.

30° or 45° thread?
Screws for plastic come with a 30° or a 45° thread flank. The 30° form puts the least radial stress on the boss and suits most appliance housings, including glass-filled grades. The 45° form has a sturdier thread and is often used in softer, more ductile plastics. Both are far gentler on the boss than a 60° sheet-metal thread, but each needs its own pilot hole size, so always use the data for the thread form you choose. Browse our thread-forming screws for plastic in 30° and 45° versions.
Designing the hole and the boss
Most cracked bosses and stripped threads start at the design stage. The pilot hole size is set as a factor of the screw's nominal diameter (d). Typical starting points for a 30° thread-forming screw are:
Pilot hole for a 30° screw
0.70 d
PP, PE
0.75 d
PA6, PA6.6, PBT, PET
0.80 d
ABS, ABS/PC, PS, PA6 GF30, PBT GF30, PET GF30
0.82 d
PA6.6 GF30
0.85 d
PC, PVC, PMMA
Typical industry guidance for 30° screws, not Fabory test data. 45° screws need their own hole sizes. For a 3.0 mm screw in ABS, 0.80 d gives a 2.4 mm pilot hole.
Four proven ways to get a strong boss

- Add a counterbore at the top of the boss to reduce stress at the entry and give a flush finish.
- Allow enough wall thickness and thread engagement for the load, using the screw maker's boss dimensions.
- Tie tall bosses to the housing wall with ribs or gussets, and avoid thick sections that cause sink marks.
- Keep weld lines, where two flows of plastic meet in the mould, away from the boss. A boss with a weld line splits far more easily.
Keeping the joint tight
Appliances vibrate and heat up, and plastic relaxes under load over time. Motors, pumps and heating elements all work joints loose, and a joint that was overtightened on the line is already weakened. Control the assembly process:

Torque window
Set tightening torque between the driving torque and the stripping torque. A strip-to-drive ratio of 3 to 1 or higher is a typical target for thread-forming screws.
Driving speed
Use torque-controlled tools at moderate speed, typically 300 to 800 rpm. Higher speeds can melt thermoplastic and weaken the thread.
Repeat assembly
Thread-forming screws can be reinstalled only a limited number of times, and holding power drops each time.
Drive type
Hexalobular (TX) drives resist cam-out and suit automated assembly. Common drives such as TX and PZ also help meet EU Ecodesign repair requirements.
Material effects to plan for
- Heat and creep: plastic loses clamp load faster at higher temperatures. Near heating elements, motors and hot water, allow more thread engagement or use a threaded insert.
- Moisture in nylon: PA6 and PA6.6 absorb moisture after moulding, which changes drive and strip torque. Set and validate torque on conditioned parts, not dry-as-moulded ones.
- Stress cracking: PC and ABS can crack in contact with some lubricants, cleaners and thread coatings. Check that anything on the screw or in the assembly process is compatible with the plastic.
Read more in the critical role of vibration-resistant fasteners.
When a screw is not the best choice
- Panels opened often in service: use threaded inserts, such as heat-set or press-in brass inserts, with machine screws. This also helps meet EU Ecodesign rules that require spare parts to be replaceable with common tools.
- Plastic parts fixed to thin sheet metal: self-drilling screws or rivets and rivet nuts may suit the metal side better.
- Earthing points: never rely on a screw in plastic to carry a protective-earth connection. IEC/EN 60335-1 Clause 28 requires screws that transmit contact pressure to screw into metal. Read our guide to earthing fasteners for electrical appliances.
Plastic housing joint checklist
- Screw type chosen for the plastic: thread-forming for thermoplastics, thread-cutting for thermosets
- No standard sheet-metal screws in plastic bosses
- Hole size taken from the screw maker's data for the material
- Boss with counterbore, enough wall and engagement, and support ribs
- Torque window specified and controlled in assembly, at moderate speed
- Threaded inserts used where panels are opened in service
- Drive, strip and pull-out tests done on production parts
Frequently asked questions
Can I use a normal self-tapping screw in plastic?
It may hold in some soft plastics, but its 60° thread puts high radial stress on the boss and raises the risk of cracking, especially in glass-filled or brittle grades. A screw designed for plastics is the safer choice.
What is the difference between thread-forming and thread-cutting screws?
A thread-forming screw displaces the plastic to form a thread without removing material, which gives high pull-out strength in thermoplastics. A thread-cutting screw removes material like a tap, which suits brittle thermosets that would crack if the plastic were displaced.
What pilot hole size should I use for a screw in plastic?
It depends on the screw and the material. For a 30° screw, most thermoplastics need a pilot hole of 0.70 to 0.85 times the screw's nominal diameter. 45° screws need their own sizes. Use the screw maker's data and confirm by testing.
How many times can a thread-forming screw be reused?
Only a limited number of times, and holding power drops each time. Use threaded inserts where a panel is opened regularly.
What torque should I use for screws in plastic?
Set the tightening torque between the driving torque and the stripping torque measured in your own parts. A strip-to-drive ratio of 3 to 1 or higher gives a safe window for production.
Why do plastic bosses crack after assembly?
The most common causes are a hole that is too small, a boss wall that is too thin, a screw with a 60° thread, or overtightening. Cracks can also appear later as the plastic relaxes or meets chemicals and heat in service.
Related reading
Need help choosing?
Fabory's engineers help appliance manufacturers select screws for plastic housings against their design and test requirements, and our accredited laboratory can verify product characteristics.
Creating peace of mind.