text.skipToContent text.skipToNavigation

Fabory | Masters in Fasteners

Earthing fasteners for electrical appliances – materials, contact and best practice

The fasteners in a protective-earth connection are safety parts. If the joint loosens, corrodes or never makes proper contact, accessible metal parts of an appliance can become live under a fault.

Choosing them well comes down to four things: the right material, the right finish, clean metal-to-metal contact and a joint that stays tight for the life of the product.

Earthing basics

Why earthing joints need different thinking

Most joints only have to hold parts together. An earthing joint also has to carry fault current with very low resistance, every time, for the life of the appliance. Its performance depends on more than the fastener alone:

  • Fastener material and coating
  • The finish of the mating parts, including paint and powder coating
  • Contact area and contact pressure
  • Dissimilar metal combinations and the risk of galvanic corrosion
  • Locking against vibration and thermal cycling
  • Tightening torque and how it is controlled on the line
  • Operating environment, including moisture and temperature

A joint that is fine on day one can still drift out of specification in service if any of these factors is overlooked.

Production testing

How earthing joints are tested

Earth continuity is checked on the production line with an earth-bond test. A typical routine test for appliances to EN 60335-1 uses a test current above 10 A from a source below 12 V.

The usual fail limit is 0.1 Ω for products without a supply lead and 0.2 Ω for products fitted with one. Every contact surface and fastener in the earth path adds to that resistance, so the margin can be small.

Routine test settings vary by product and test equipment. Always check the limits against the current standard and the part 2 for your appliance type.

Standards and requirements

What IEC/EN 60335-1 covers

For household and similar appliances, IEC/EN 60335-1 sets the rules in Clause 27 (Provision for earthing) and Clause 28 (Screws and connections). Among other things, these cover:

  • Securing earthing terminals against accidental loosening
  • Avoiding corrosion where dissimilar metals meet, such as copper and aluminium
  • Making sure contact pressure is not carried through insulating material that can shrink or creep

Design to the current edition of the standard and the part 2 for your appliance type, and confirm the final design by testing.

Material selection

Choosing the material and finish

The right material balances conductivity, strength and corrosion resistance with the parts it touches.

Material or finishStrengthsWatch out forTypical use
BrassGood conductivity and corrosion resistanceLower strength than steel; do not over-torqueTerminal screws, earthing studs, nuts on busbars
Plated brass (tin or nickel)Stable, low contact resistanceThe plating must suit the mating terminalTerminals and connections to copper conductors
Zinc-plated steelHigh strength, low cost, widely availableFinish and passivation affect contact resistanceChassis earthing points, sheet-metal joints
Stainless steel (A2, A4)Excellent corrosion resistanceHigher resistivity; galling in stainless-on-stainless threadsOutdoor units and damp environments

Choose the finish together with the mating parts. Where copper and aluminium meet, use a suitable intermediate material or plating to prevent galvanic corrosion.

Contact surfaces

Making contact through paint and coatings

Painted or powder-coated panels are the most common cause of high earth resistance. The coating insulates the joint even when the screw is fully tight, so every earthing point needs a deliberate route to bare metal.

Appliance manufacturers use three proven methods.

Quick comparison

Contact methods at a glance

01

Mask or remove the coating

Mask the earthing point before coating, or remove the coating locally, so the terminal clamps directly onto the base metal.

02

Toothed or serrated lock washers

DIN 6797 and DIN 6798 type washers bite through thin coatings into the base metal as they are tightened.

03

Dedicated earthing studs

A stud welded or clinched into the chassis gives a fixed earthing point, with the ring terminal clamped between washer and nut.

Vibration and thermal cycling

Keeping the joint tight

Appliances vibrate and heat up. Motors, pumps, compressors and heating elements all work joints loose over time, and every loss of clamping force raises contact resistance. Use a locking method suited to the joint and its operating temperature:

  • Nord-Lock wedge-locking washers, which secure through clamp tension rather than friction
  • DIN 985 nylon-insert locking nuts for general assembly areas
  • All-metal locking nuts, such as ISO 7042 or DIN 980, near heating elements, oven cavities, compressor heads and other hot zones
  • Thread-locking adhesives or pre-applied patches, which also seal the thread against moisture; use high-temperature grades near heat sources

Nylon inserts and standard threadlockers have temperature limits, so check the specification against the maximum operating temperature of the joint. Control tightening torque on the line too, especially with brass, which strips more easily than steel.

More about vibration-resistant fasteners ›

Avoiding failures

Common mistakes with earthing joints

Most failed earth-bond tests in production come down to a small number of avoidable causes:

  • Clamping a terminal onto painted or powder-coated metal
  • Letting copper and aluminium touch without protection
  • Carrying contact pressure through a plastic part or insulating washer
  • Relying on friction alone in a joint exposed to vibration
  • Using nylon-insert locking nuts near heating elements or other hot zones
  • Overtightening brass screws and stripping the thread
  • Choosing a plating that does not suit the mating terminal
  • Not specifying tightening torque, or not controlling it in assembly
  • Reusing toothed washers that have already been flattened

Each of these can pass a first test and still fail later, so build the checks into both design review and production testing.

Before release

Earthing joint checklist

  1. Conductive material and finish chosen to suit the mating parts
  2. No unprotected contact between copper and aluminium
  3. Bare metal contact at every earthing point
  4. Locking method that resists vibration and thermal cycling, rated for the operating temperature
  5. Tightening torque specified and controlled in assembly
  6. Earth-bond test included in production testing

Technical questions answered

Frequently asked questions about earthing fasteners

Answers to the questions appliance designers ask most about protective-earth connections.

Can I use a stainless steel screw for an earthing connection?

Yes, if the joint is designed for it. Stainless steel resists corrosion well but has higher resistivity than brass, so check the joint resistance by testing.

Do toothed lock washers stop a joint loosening?

They help make contact through thin coatings, but on their own they are not a reliable anti-vibration solution. Combine them with a proven locking method where the joint is exposed to vibration.

Can I use nylon-insert locking nuts near heating elements?

Not in hot zones. The nylon insert has a temperature limit, so near heating elements, oven cavities and compressor heads use all-metal locking nuts such as ISO 7042 or DIN 980, or wedge-locking washers. Check the specification against the maximum operating temperature of the joint.

Can I earth through a thread-forming screw in sheet metal?

It is common, because the formed thread gives good metal contact. Make sure the hole size, sheet thickness and torque give a full, tight thread, and confirm the resistance by testing.

Which standard covers earthing in household appliances?

IEC/EN 60335-1, mainly Clause 27 (Provision for earthing) and Clause 28 (Screws and connections), together with the part 2 for the specific appliance type.

Why does my appliance fail the earth-bond test when the screw is tight?

The most common cause is a coating between the terminal and the chassis. Check for paint or powder coating at the contact point, then check for corrosion or an unsuitable plating.

Ask our technical specialists

Fabory | Masters in Fasteners

Need help with an earthing joint?

Earthing joints combine electrical, mechanical and corrosion requirements, and the right choice depends on your design, materials and production process.

Fabory's engineers help appliance manufacturers select earthing hardware against their design and test requirements, and our accredited laboratory can verify product characteristics.

Creating peace of mind.

Do not close this page. This message will disappear, when the page is fully loaded.