Author: Carline Klijn - van Best Date: 07/09/2026
October 8 at AFAS Theater in Leusden
Are you visiting Staalbouwdag at the AFAS Theater in Leusden on 8 October? This year, Fabory will be attending the annual industry event for the Dutch steel construction sector for the first time. You can meet Tim Jost and Stef van der Linden at our stand in the foyer.
Discuss fasteners for steel construction
Tim and Stef will bring a range of fasteners for steel structures to Leusden. At the stand, you can take a closer look at SB bolt assemblies in accordance with EN 15048 and HV preloaded bolt assemblies in accordance with EN 14399-4. Threaded rods according to DIN 976, anchor rods and hook anchors will also be on display.
Do you have questions about the application or specification of these fasteners? Discuss them with our experts. They can also tell you more about cut-to-length threaded rods according to DIN 976 in various materials and finishes, including hot-dip galvanized, electroplated zinc, A2-70 and A4-70.
Bouwakkoord Staal takes centre stage
Staalbouwdag brings together clients, architects, structural engineers, contractors, steel construction companies and suppliers. In addition to the trade exhibition, the event features an extensive programme of expert sessions.
This year, Bouwakkoord Staal takes centre stage. Presentations, expert panels and discussions will explore the ambitions and agreements aimed at making the use of steel in the construction and civil engineering sectors more sustainable. The winners of the Nationale Staalprijs will also be announced during the conference.
Meet Tim or Stef on 8 October
Would you like to discuss a specific question with Tim Jost or Stef van der Linden during Staalbouwdag? Contact them in advance at tim.jost@fabory.com or stef.vanderlinden@fabory.com. This way, they will know you are coming and can reserve time to speak with you.
Staalbouwdag takes place on 8 October at the AFAS Theater in Leusden. Curious about what Staalbouwdag is like? Watch the aftermovie from the 2025 edition.