text.skipToContent text.skipToNavigation
Life & Mobility wheelchair user representing mobility and independence

At Life & Mobility in Doetinchem, efficiency, clarity and reliability are important parts of the production environment. The company develops innovative wheelchairs and mobility scooters and has introduced eleven two-bin shelving units combined with a Fabory Logic RFID Dropbox to support inventory management on the production floor.

The installation now provides more than twelve metres of two-bin shelving. When the first bin is empty, the operator places it in the RFID Dropbox. The system automatically registers consumption and triggers replenishment, while production can continue using the second bin.

Results at a glance

11

Two-bin shelving units installed on the Life & Mobility production floor.

12+ metres

Of two-bin shelving supporting inventory management in production.

Automatic

Consumption registration and replenishment are triggered through the RFID Dropbox.

Fabory Logic two-bin shelving and RFID inventory management at Life & Mobility

Simplifying inventory management on the production floor

Life & Mobility selected a combination of two-bin shelving and RFID technology to support its production process. The system is designed so that a second bin remains available when the first becomes empty.

This means employees do not need to create a manual order when a bin requires replenishment. Instead, returning the empty bin through the RFID Dropbox registers the consumption and starts the replenishment process automatically.

The approach helps maintain access to stocked items while reducing the manual work involved in managing replenishment.

How the two-bin RFID process works

1

Use the first bin

Components are taken from the first bin during normal production.

2

Return the empty bin

When the first bin is empty, the operator places it in the RFID Dropbox.

3

Replenishment is triggered

The RFID system registers the consumption and automatically triggers replenishment.

4

Continue with the second bin

Production continues using the second bin while replenishment is arranged.

Time savings and improved stock availability

Life & Mobility identifies three clear outcomes from the new system: time savings in production, prevention of shortages and a clean, well-organised workplace.

The combination of two-bin shelving and RFID-triggered replenishment removes the need for manual ordering when an empty bin is returned. The second bin remains available for production while the replenishment process is underway.

“With the new system, we save time, prevent shortages, and maintain a professional-looking workshop.”

Bastiaan van der Post
Tactical Buyer, Life & Mobility

A clean and professional production environment

The installation was designed with both function and appearance in mind. The shelving units are branded with the Life & Mobility logo, helping them fit into a professional and well-organised working environment.

A team of Fabory merchandisers carried out the installation in collaboration with Solution Engineer Raymond van Dongen. Working together with the Life & Mobility shop floor team kept disruption to a minimum, and production continued during the installation.

The result: less manual ordering and better stock availability

The eleven shelving units and RFID Dropbox provide Life & Mobility with a structured way to manage replenishment across more than twelve metres of two-bin shelving.

When a bin becomes empty, returning it through the RFID Dropbox automatically registers consumption and initiates replenishment. Employees can continue working from the second bin rather than creating a manual order.

For Life & Mobility, the result is a system that saves production time, helps prevent shortages and supports a clean and well-organised workplace.

Automated inventory replenishment

Could Fabory Logic RFID simplify your inventory management?

Fabory Logic RFID can automatically register returned bins and trigger replenishment, reducing the manual work involved in managing inventory.

Talk to a Fabory specialist Discover Fabory Logic RFID
Do not close this page. This message will disappear, when the page is fully loaded.