text.skipToContent text.skipToNavigation
Door de hoge temperaturen van de afgelopen dagen kan de bezorging door DHL langer duren dan normaal. Gebruik de Track & Trace-link in MyFabory om de zending te volgen.
Anchor calculation software interface for structural fixings in concrete

Choosing between HV and HR assemblies starts with understanding the connection requirement

In steel construction, HV and HR assemblies are both associated with high-strength structural bolting for preloaded connections. They are often discussed together, but they are not interchangeable by assumption.

The selected assembly affects how the connection is specified, how installation is approached and how the project team manages compliance and documentation. That is why the distinction matters for engineers, buyers and QA teams from the outset.

Understanding the difference between HV and HR assemblies helps reduce uncertainty and supports more confident structural bolting decisions across the project lifecycle.

The right assembly choice supports performance, installation confidence and compliance

In preloaded structural connections, small assumptions can create large project problems. Choosing the wrong assembly type, mixing components incorrectly or overlooking installation expectations can lead to delay, rework or uncertainty during inspection and handover.

HV and HR assemblies matter because they sit within a controlled structural bolting context. The product is only one part of the answer. The full assembly, the tightening method and the specification route all play a role in the final connection performance.

For project teams, understanding the distinction helps reduce risk and supports smoother execution from specification through to supply and installation.

What HV and HR assemblies refer to

HV and HR assemblies are high-strength structural bolting assemblies used in preloaded steel construction connections. They are designed to be used as complete assemblies rather than as individual components selected in isolation.

In practice, the distinction between HV and HR depends on the assembly system and the specified product route. That is why selection should always follow the project requirements and the defined assembly type, not just bolt size or strength class.

HV vs HR

The main difference is not simply about the bolt on its own. It is about the assembly system being specified and used as part of a preloaded structural connection.

HV = a defined high-strength structural bolting assembly system

HR = a different defined high-strength structural bolting assembly system

The simplest way to understand the difference is that HV and HR are not just labels applied to individual bolts. They refer to different assembly routes within high-strength structural bolting for preloaded applications.

That affects how the full assembly is selected, how the components are matched and how the project team approaches installation and control. The complete assembly, not a single item in isolation, should always drive the decision.

A common mistake is to treat HV and HR as alternative names for the same thing. They are not. They should be treated as specific assembly systems with their own specification route.

What HV and HR assemblies have in common

Both HV and HR assemblies are used for high-strength structural bolting in preloaded steel construction connections.

Although they are different assembly systems, HV and HR assemblies share some important ground. Both are associated with controlled structural bolting where the project requires a preloaded connection and where the full assembly matters to the intended performance.

• both are used in preloaded structural connections
• both rely on correct assembly selection
• both require attention to installation practice
• both need the correct bolt, nut and washer combination
• both form part of a wider compliance and documentation route

HV and HR assemblies at a glance

Topic HV HR
Main role Defined high-strength structural bolting assembly for preloaded use Defined high-strength structural bolting assembly for preloaded use
Key distinction Specific assembly route Different specific assembly route
Selection focus Correct complete assembly and project specification match Correct complete assembly and project specification match
Installation relevance Installation method and control matter Installation method and control matter
Main risk if misapplied Wrong assembly route or component mix can affect compliance and function Wrong assembly route or component mix can affect compliance and function

When HV assemblies should be used

HV assemblies should be used where the project specification or structural design clearly calls for the HV assembly route.

HV should be treated as a specified assembly choice rather than a product substitution option.

HV assemblies are the correct route where the project requirement identifies HV specifically and where the full assembly, installation practice and documentation route are aligned to that system. The decision should always come from the design and specification, not from what appears close in stock.

HV is especially relevant where:
• the project specification identifies HV assemblies
• the design requires a preloaded structural bolting assembly
• the full assembly can be supplied and installed as specified
• documentation and compliance control need to match the HV route

When HR assemblies should be used

HR assemblies should be used where the project specification or structural design clearly calls for the HR assembly route.

HR should be treated as its own specified assembly choice and not assumed to be a like-for-like alternative to HV.

HR assemblies are the correct route where the project requirement identifies HR specifically and where the project team can align supply, installation and documentation to that system. As with HV, the choice should come from the specification and application need rather than visual similarity or stock convenience.

HR is especially relevant where:
• the project specification identifies HR assemblies
• the design requires a preloaded structural bolting assembly
• the full assembly can be supplied and installed as specified
• documentation and compliance control need to match the HR route

What buyers, engineers and QA teams should check

Before ordering HV or HR assemblies, it is worth checking the specified assembly type, preload requirement, complete component set, installation route and documentation needs.

Correct selection is about the full structural bolting route, not only the bolt itself.

1

What does the project specification call for?

The first check should always be whether the project identifies HV or HR specifically. That should lead the decision.

2

Is the full assembly correct?

Bolt, nut and washer combination matters. Structural bolting assemblies should not be reduced to a single component choice.

3

Does the connection require preload?

HV and HR assemblies sit within preloaded structural bolting, so the design requirement for preload should already be clear.

4

How will installation be controlled?

Tightening method, assembly integrity and project control all matter in preloaded structural connections.

5

What documentation is required?

In steel construction, standards alignment, traceability and document readiness can all be important to audits, QA review and final handover.

Common mistakes to avoid

Problems usually start when HV and HR assemblies are treated as product labels rather than specific structural bolting systems.

Assuming HV and HR are interchangeable

They are not. Each is a defined assembly route and should only be used in line with the project specification.

Ordering by bolt characteristic alone

A structural bolting assembly should never be reduced to one component or one visible attribute.

Mixing components incorrectly

Incorrect bolt, nut and washer combinations can affect both compliance and intended function.

Overlooking installation and documentation control

In preloaded connections, the installation route and documentation pack are part of the wider performance and compliance picture.

How Fabory supports the right selection

The right support goes beyond supply alone. It also means helping customers manage specification, documentation and project continuity with greater confidence.

Fabory helps customers reduce uncertainty around structural bolting selection, assembly compliance and documentation readiness.

Fabory supports steel construction customers with more than product availability alone. The wider approach is built around helping teams choose the correct structural bolting route while keeping standards, installation expectations and documentation needs in view.

Fabory support can include:
• support for structural bolting selection aligned to specification
• availability and dependable supply
• support for engineers, buyers and QA teams
• guidance around documentation and project readiness
• a more complete route to steel construction support

The aim is to help customers make more confident HV and HR assembly decisions with fewer avoidable project issues.

Related topics worth exploring

HV and HR assemblies sit alongside wider questions about structural bolting standards, documentation and compliant project execution.

EN 15048 vs EN 14399
Certificates and documentation in steel construction
ETA and DoP explained for anchoring systems
Threaded rods and studs in steel construction
Anchoring steel to concrete

Need support with HV or HR assemblies in steel construction?

Talk to Fabory about structural bolting selection, documentation support and the right route for compliant steel construction supply.

Talk to Fabory
Sluit deze pagina niet. De melding verdwijnt zodra de pagina klaar is met laden.