text.skipToContent text.skipToNavigation
*Until further notice, all orders placed will be coming from the Netherlands, with an estimated lead time of 5 days*
Header Food&Dairy

Choosing the Right Stainless Steel Fasteners for Your Needs

If you work in machine building for the food industry, you likely have standard stainless steel plates, profiles, and fasteners in stock. After all, without the correct fasteners, machines cannot function. So, why do so many companies choose stainless steel for their machinery? Here are some reasons:

  • Strength: Stainless steel is a robust material that can withstand significant stress.  
  • Corrosion Resistance: It is highly resistant to rust and corrosion, making it ideal for various environments.  
  • Ease of Cleaning: Stainless steel's smooth surface allows for easy cleaning, which is crucial in food processing.  
  • Hygienic and Food Safe: Stainless steel is non-reactive and safe for food contact, ensuring the safety of processed products.  
  • Durability and Low Maintenance: It offers long-lasting performance with minimal maintenance requirements.
Food&Dairy

Most Commonly Used Fasteners in the Food Industry

Which fasteners do we see the most on the order lists of customers from the food industry?

The Fabory range includes more than 30,000 stainless steel fasteners, which you can order from stock on Fabory.com. Can't find the product you are looking for in the overview? Please let us know, and we will deliver it to you. In addition, we design and manufacture the product ourselves if it does not already exist.
 

Discover our range of stainless steel

Lubrinox: Pre-lubricated Bolts, Screws, and Nuts

Fabory has developed a new line of fasteners known as Lubrinox bolts, nuts, and screws. When using stainless steel fasteners, it is common for the inner and outer threads to seize together, making it difficult to loosen them. While applying a paste can prevent this issue, it requires additional time, and the workpieces and hands must be cleaned afterwards. Lubrinox has been specifically designed for the food industry to provide long-lasting lubrication in connections.

Below are the key advantages of Lubrinox:

  • Prevents galling of stainless steel bolt connections
  • Approved for use in the food industry
  • Pre-applied at Fabory, saving an average of 25 seconds per connection
  • Available in nuts as well
  • Maintains the stainless steel appearance of articles
  • Works effectively in combination with Loctite
  • Eliminates the issue of dirty hands from manual lubrication

Manufacturer of Coolers and Dryers

Geelen Counterflow, a design and production company based in Haelen, is one of the first to test Lubrinox. The lubricated fasteners are incorporated into coolers and dryers specially designed for the food industry. Geelen Counterflow ships several units of these coolers and dryers weekly to locations worldwide.

Due to the extensive use of stainless steel fasteners, the company sought a cost-effective alternative to traditional lubrication methods. René Derckx, the technical purchaser at Geelen Counterflow, stated, “We were curious whether the solution developed by Fabory would meet our needs. The primary requirement was to prevent threads from getting stuck. We wanted to avoid having to cut or drill out a screw.

Another coating that employees frequently use is significantly thicker. However, the Lubrinox fasteners do not require such a substantial layer. “A thick layer makes it difficult to drive screws by hand, causing them to become overly greasy. If you need to exert force, your fingers tend to slip over the hex. That doesn’t happen with Lubrinox. The feedback from the shop floor during this test has been positive,” he added.

Lubrinox
Stainless steel fasteners go into the Counterflow Cooler Plus
Captive screws & bolts

Captive screws and bolts

Nobody wants to find a screw or bolt at the end of the chain in the food. At the same time, fixing fasteners in panels and doors that open and close regularly is a challenge. The Fabory range includes captive screws and bolts fitted with a space-saving clip. This space-saving locking clip eliminates the need to leave space for a locknut behind the panel. The screws have a reduced shank, so you no longer have to tap threads into the holes in the panel. We worked out this innovative solution together with a customer who came up with this idea. Does your application also require a specific extension of the range? We would be happy to work with you. Contact us.

Hygienic bolts and nuts

As a food producer, you want to periodically clean and disinfect machines. In washdown machines, you need fasteners with specific design features such as smooth surfaces and minimal voids. We have developed it for you. The Fabory Premium Stainless Hygienic fasteners (FPS-H) from Fabory have a smooth and polished surface and rubber sealing rings.

Personal advice on your fastening challenges?

FDA, Hygiene, Machinery safety, corrosion resistance, our Application Engineers contribute solutions and provide advice on fasteners, the design and application of various fasteners. Our close cooperation with standardization institutes and technical committees guarantees a high level of technical knowledge, information and service!

Optimising Processes Together

Fasteners may be a conservative product category, but we at Fabory are committed to continuous innovation. The food industry has trusted Fabory for years to supply stainless steel fasteners because:

  • Our fasteners are designed to enhance efficiency and comply with industry regulations.
  • Smart logistics solutions optimise fastener stock management and reduce the Total Cost of Ownership (TCO), leading to greater flexibility and cost control within your organisation.
  • Our Peace of Mind solutions ensure that production operations run smoothly.

Creating Peace of Mind

Fabory offers an extensive selection of over 120,000 fasteners in various designs, sizes, and materials. Managing such a large inventory requires reliable systems. Our smart logistics solutions provide insights into consumption patterns, significantly assisting inventory management. With our RFID solution and Weight Scale Cabinet, you can access your Vendor Managed Inventory (VMI) monitor in MyFabory, offering insights into historical consumption and our performance. The combination of tailored solutions and actionable insights is genuinely unique.

Our Application Engineers are here to provide solutions and expert advice on fasteners, designs, and applications. In addition to these services, Fabory's experts conduct calculations and tests to ensure secure connections. We collaborate closely with standardisation bodies and technical committees to maintain high technical knowledge and support. This commitment fosters Peace of Mind, allowing you and your team to focus on your core tasks.

Please get in touch with us to explore the possibilities further.

Food_Process.png

Masters in Fasteners

Assortment

Fabory is the ideal choice for all your fastening needs. Our product portfolio includes a wide range of standard fasteners and custom solutions for various applications, complemented with C-parts.

Fabory Logic

Fabory helps you access Fasteners and C-parts and uses innovative dashboards to provide insights into your consumption, helping you reduce your TCO. Fabory Logic offers RFID, Optical-Eye, Weight Scales, and Merchandiser services.

QA/QC & Engineering

Fabory prioritises quality and reliability, strongly emphasising refined quality management and specialised control systems to support your fastener selection.

Do not close this page. This message will disappear, when the page is fully loaded.