text.skipToContent text.skipToNavigation
Header TTC.pngTruck, Trailer & Coach Building

The Right Fasteners for Every Situation

If you are involved in the Truck, Trailer, and Coach Building industry, you understand the importance of considering factors such as the environment, quality, reliability, uptime, safety, and punctuality. To meet the needs of this industry, we operate based on a stock principle, offering a range of standard fasteners. If a standard fastener does not meet your requirements, we can develop a custom solution and collaborate with our production partners. Additionally, we provide relevant C-parts and MRO parts, including tools, safety equipment, electronics, and hydraulic and pneumatic components.

Your TCO down

Effective inventory management is crucial in production, as waste must be minimised. Excess inventory can reduce profitability, while insufficient stock can cause production delays. Fabory offers smart logistics solutions for managing maintenance, repair, and production stock, helping you optimise inventory management and lower your Total Cost of Ownership (TCO). This approach enhances flexibility and cost control within your organisation.

Most ordered fasteners in Truck, Trailer & Coach Building

Which fasteners are most commonly found on our customers' order lists in this industry? The six fasteners listed below are the most frequent. They are primarily made of carbon steel and are treated with corrosion protection methods such as electrolytic galvanising and zinc flake coating.

Zinc Flake Fasteners for Truck, Trailer and Coachbuilding

Clamping Load Distribution with Flange Bolts and Flange Nuts

Distributing the clamping load effectively without using additional washers can be done by utilising strong fasteners like flange bolts and flange nuts, which are manufactured as a single piece. The non-serrated rim of these fasteners is robust enough for most applications. At the same time, the toothed edge is ideal for industrial settings that experience heavier loads, as it is self-locking and more resistant to vibrations.

By eliminating the need for washers, flange bolts and nuts can be tightened more quickly and efficiently than many other bolts. This offers several advantages, including:

  • Reduced labour costs
  • Increased productivity
  • Easier installation in hard-to-reach or narrow spaces
  • More efficient management

Our range of flange fasteners is made from different grades of carbon steel, including screws in classes 8.8 and 10.9, and nuts in classes 8 and 10, all with a surface treatment of galvanised zinc flakes. Stainless steel screws and nuts are also available in A2 and A4 classes.

Discover our range of flange bolts and flange nuts.

Fasteners with zinc flake coating

Corrosion protection is a much-discussed topic in the Truck, Trailer & Coachbuilding industry. Not surprisingly, because functional parts are exposed to high loads, the parts must also be protected against external influences and corrosion. Therefore, different coatings are available. The most common coating is zinc flake, a coating consisting of zinc and aluminium flakes connected by an inorganic matrix. The need for fasteners with a zinc flake surface coating was increasing, and because production in the Truck, Trailer & Coachbuilding industry must never stagnate, we supply 2,000 articles in zinc flake from stock.

The benefits of zinc flake at a glance:

  • High corrosion resistance
  • Thin layer
  • Also suitable for high tensile steel
  • No hydrogen embrittlement
  • Some degree of electrical conductivity
  • Suitable for all shapes and sizes
  • Hexavalent chromium (Cr6+) free

Hundreds of zinc flake fasteners disappear in every trailer: in the chassis, the floor frame, the superstructure and various trailer components. 

Discover our zinc flake range

Zinc Flake Fasteners for Truck, Trailer and Coach Manufacturing

Case Study: Knapen Trailers

Knapen Trailers from Deurne in Brabant uses a unique variation of zinc flake fasteners from Fabory. Employees reach for thousands of Fabory articles with a zinc flake treatment every week on the shop floor of the producer of moving floor trailers. Johan van Hommelen, a strategic purchaser at Knapen Trailers, explains that the corrosion resistance of the fasteners is a crucial factor for the company. “Our trailers, and therefore also the fastening materials used, are exposed to wind and weather year after year. The influence of the weather on the materials is significant.”

Hundreds of zinc flake fasteners disappear in every trailer: the chassis, the floor frame, the superstructure and various trailer components. The stock management of the zinc flake fasteners remains stable thanks to an RFID solution. “The complete ordering process, including that of the zinc flake fasteners, is taken care of”.

Fasteners and C-Parts Selected for Truck, Trailer and Coach Building
Logic Inventory Managment

Blind Riveting

Blind riveting is a widely used fastening technique in truck, trailer, and coach building. This method is employed in nearly every bus, truck, and trailer, including components such as the cab, seats, chassis, roof rails, safety structures, floor systems, and more.

Depending on the specific application, a standard blind rivet or a blind rivet nut may be suitable. Fabory offers structural blind rivets and lockbolts for critical applications within this industry.

Discover our blind riveting range.

Hose Clamps

Hose clamps are essential throughout the Truck, Trailer, and Coachbuilding industry. We offer a variety of hose clamps suitable for different applications, including:

  • Air intake and induction systems
  • Cooling systems
  • Exhaust systems
  • Turbocharger installations
  • Fuel and oil systems

Our selection includes carbon steel, stainless steel alloys, worm gear clamps, ear clamps, two-piece clamps, spring clamps, and heavy-duty options. No matter the specific requirement, we have the proper clamp (such as ABA, Norma, or MaxxFast) for every hose.

Discover our hose clamp range.
 

More Than Just Fasteners

At Fabory, we specialise not only in fasteners but also in a range of production components. Our offerings include cable ties, sealants and lubricants, electrical components, hydraulics and pneumatics, safety equipment, and tools.

Intelligent management of C-parts is becoming increasingly important. By working closely with our customers and suppliers, we create a customised range of products, services, and expertise to meet specific needs.

  • ABB cable ties
  • Ripca electronic components (cable, terminals, connectors)
  • OXXA safety equipment
  • Henkel / Loctite adhesives, sealants and surface treatments
  • 3M adhesives, abrasives
  • Motip technical sprays, additives
  • WD40 lubricants, degreasers, rust removers
  • Bosch power tools
  • Sonic Hand Tools

View our full range on the webshop

Logo's

Creating Peace of Mind

At Fabory, you can choose from over 120,000 fasteners in various designs, sizes, and materials. Such a vast selection requires efficient inventory management that you can depend on. Our innovative logistics solutions offer insights into consumption, helping you manage your inventory effectively. With our RFID solution and Weight Scale Cabinet, you can access your Vendor Managed Inventory (VMI) monitor within the MyFabory environment. This tool provides valuable insights into the historical consumption of your stock and our performance. The unique combination of offering solutions and providing insights sets us apart.

In addition to these solutions, Fabory's experts are available to offer advice, calculations, and testing to ensure secure connections. This gives you peace of mind, allowing you and your employees to focus on your core tasks.

Masters in Fasteners

Assortment

Fabory is the ideal choice for all your fastening needs. Our product portfolio includes a wide range of standard fasteners and custom solutions for various applications, complemented with C-parts.

Fabory Logic

Fabory helps you access Fasteners and C-parts and uses innovative dashboards to provide insights into your consumption, helping you reduce your TCO. Fabory Logic offers RFID, Optical-Eye, Weight Scales, and Merchandiser services.

QA/QC & Engineering

Fabory prioritises quality and reliability, strongly emphasising refined quality management and specialised control systems to support your fastener selection.

Do not close this page. This message will disappear, when the page is fully loaded.