text.skipToContent text.skipToNavigation
News banner_Updates from Fabory
Jochem Oerlemans - Product Category manager at Fabory

    Author: Jochem Oerlemans                                   Date: 04/06/2026

Lubrinox Range Expands with More than 1,200 New Articles

Fabory has significantly expanded its Lubrinox portfolio, adding more than 1,200 new stainless steel fasteners to the range. The expansion makes it easier than ever for manufacturers, machine builders, and maintenance professionals to benefit from a fastening solution designed to eliminate galling while improving assembly efficiency. Lubrinox is Fabory's innovative range of pre-lubricated stainless steel fasteners. Each fastener is supplied with a specialised high-performance coating that reduces friction, prevents cold welding (galling), and delivers more consistent installation performance compared to conventional stainless steel fasteners.

Responding to Growing Industry Demand

As stainless steel fasteners continue to be specified across industries such as food processing, machine building, petrochemical, medical equipment, and infrastructure, the challenges associated with galling remain a common issue. Fasteners that seize during installation can lead to damaged components, increased assembly time, maintenance difficulties, and costly downtime. The expanded Lubrinox range provides engineers and buyers with access to a wider selection of the most commonly specified stainless steel fasteners while maintaining the same anti-galling performance that has made Lubrinox increasingly popular across Europe.

Why Lubrinox?

Unlike traditional stainless steel fasteners that often require additional lubrication during assembly, Lubrinox fasteners arrive ready to install.

Key benefits include:

  • Reduced risk of galing & cold welding
  • Faster and more consistent assembly,
  • No need for additional lubricants,
  • Clean, dry installation without contamination,
  • Suitable for use with thread-locking compounds,
  • Food-grade compliant coating,
  • Full batch traceability

By eliminating the need for manual lubrication, Lubrinox helps manufacturers improve productivity while reducing Total Cost of ownership with reduced assembly variation and operational costs.

Specialist in building machines automating processes in the food industry, Viscon, is a perfect example of this. Updating their stainless steel fasteners to Lubrinox allows for a shortened installation process and reliable performance. Discover the full benefits experienced by Viscon 

Greater Choice, Same Proven Performance

The addition of more than 1,200 new articles means customers now have access to an even broader selection of Lubrinox products across popular standards and dimensions. The expanded range supports both OEM production environments and maintenance operations where reliability, efficiency, and ease of installation are critical. For customers seeking maximum protection against galling, Fabory continues to recommend combining Lubrinox-coated bolts with Lubrinox-coated nuts, delivering optimum anti-seize performance throughout the assembly.

Supporting Reliable Production

As manufacturers continue to focus on reducing downtime and improving process efficiency, fastener solutions play a more important role than ever. With the expanded Lubrinox range, Fabory is helping customers simplify assembly process, reduce maintenance challenges, and improve long term reliability across a wide range of applications. The full Lubrinox range is available now through the webshop, or from your Fabory contact.

Do not close this page. This message will disappear, when the page is fully loaded.