text.skipToContent text.skipToNavigation
Anchor calculation software interface for structural fixings in concrete

Choosing the right anchor starts with understanding how the fixing needs to perform

In steel construction, selecting between a mechanical anchor and a chemical anchor is not simply a matter of installer preference. The right choice depends on the application, the substrate, the load case and the wider project requirement.

Both anchor types can play an important role in steel-to-concrete fixing, but they work in different ways and bring different installation and documentation considerations with them. That distinction matters for performance, compliance and project continuity.

For engineers, buyers and QA teams, understanding the difference helps reduce risk and supports more confident anchor selection from specification through to supply and installation.

Anchor selection affects more than installation speed

In steel construction, anchor selection can influence load performance, installation method, inspection confidence and final documentation. A fixing that appears suitable at first glance may not be the right answer once the full application is considered.

Mechanical and chemical anchors behave differently in concrete. They respond differently to edge distances, spacing conditions, hole preparation, curing expectations and the wider installation environment. That means the decision should always be led by the application, not by habit.

For project teams, the right choice helps reduce uncertainty and supports smoother execution from product selection through to site installation and handover.

What these two anchor types refer to

Mechanical anchors are fixing systems that transfer load through a mechanical action in the concrete, such as expansion, interlock or undercut behaviour depending on the anchor type. They are often associated with fast installation and immediate loadability.

Chemical anchors use a bonded installation method, typically with resin and a threaded element, to achieve the fixing in concrete. They are often selected where reduced expansion forces, installation flexibility or specific anchoring conditions are important.

Mechanical vs chemical anchors

The main difference is how the anchor transfers load into the concrete and what that means for installation and application suitability.

Mechanical anchors = load transfer through mechanical action

Chemical anchors = load transfer through bonded installation

The simplest way to understand the difference is to focus on how the fixing works inside the concrete. Mechanical anchors rely on the anchor design creating a secure mechanical hold. Chemical anchors rely on resin bonding the threaded element into the prepared hole.

That difference affects installation speed, edge and spacing sensitivity, hole preparation requirements and how the anchor behaves in different site conditions. Neither route is automatically better. The correct answer comes from the application.

A common mistake is to treat the choice as purely a product preference. In reality, it is a project-specific decision about fixing.

What mechanical and chemical anchors have in common

Both anchor types are used to create secure steel-to-concrete fixings, and both need to be selected in line with the application and project requirement.

Although they work differently, mechanical and chemical anchors share some important ground. Both can form part of approved fixing solutions, both depend on correct installation and both need to be matched to the actual load case and substrate condition.

• both are used for steel-to-concrete fixing
• both must match the load case and substrate
• both rely on correct installation practice
• both may involve documentation or approval checks
• both should be chosen from the project requirement, not convenience alone

Mechanical and chemical anchors at a glance

Topic Mechanical anchors Chemical anchors
Main principle Mechanical locking or expansion Bonded installation using resin
Installation Often faster and immediately loadable Requires correct hole preparation and cure control
Edge and spacing relevance Can be more sensitive depending on anchor type Often preferred where reduced expansion forces are useful
Typical strength of choice Installation speed and immediate fixing Flexibility and bonded anchor performance
Main risk if misapplied Incorrect torque, spacing or substrate match can affect performance Poor cleaning, temperature control or curing can affect performance

When mechanical anchors should be used

Mechanical anchors are often the right route where the application benefits from fast installation and immediate loadability, provided the substrate and design conditions suit the anchor type.

Mechanical anchors are typically selected where installation efficiency and a robust mechanical fixing route are important.

Mechanical anchors are generally the right direction where the connection design, spacing conditions and substrate suitability align with the anchor type being considered. They are often relevant where the project benefits from quicker installation and where curing time would be less desirable.

Mechanical anchors are especially relevant where:
• fast installation is important
• immediate load application is preferred
• spacing and edge conditions suit the anchor design
• the selected product is approved and suitable for the intended use

When chemical anchors should be used

Chemical anchors are often the right route where the application benefits from a bonded fixing solution, reduced expansion forces or more flexibility around embedment and installation conditions.

Chemical anchors are typically selected where the project needs a bonded anchor solution and can manage the installation controls that come with it.

Chemical anchors are generally the right direction where reduced expansion stress, flexible embedment depth or specific anchoring conditions make them more suitable than a mechanical route. They are especially relevant where the application can support correct cleaning, installation temperature control and curing management.

Chemical anchors are especially relevant where:
• reduced expansion forces are preferred
• a bonded threaded rod installation is required
• installation flexibility is useful
• the site can control preparation and curing conditions properly

What buyers, engineers and QA teams should check

Before ordering anchors, it is worth checking the load case, substrate condition, spacing and edge requirements, installation route and documentation needs.

Correct anchor selection depends on the real application conditions, not just on hole diameter or fixing preference.

1

What does the application require?

The decision should begin with the actual fixing requirement, including load direction, substrate condition and connection design.

2

What is the concrete condition?

Cracked or non-cracked concrete, base material quality and substrate thickness all affect anchor suitability.

3

Do spacing and edge distances matter?

These conditions can be especially important when deciding whether a mechanical or chemical route is more suitable.

4

Can the chosen anchor be installed correctly on site?

Torque control, hole cleaning, curing time and environmental conditions all matter depending on anchor type.

5

What documentation or approval route is required?

In approved or compliance-sensitive projects, documentation and declared product suitability can be just as important as the fixing itself.

Common mistakes to avoid

Anchor problems usually begin when teams simplify the decision too early or overlook the installation conditions behind the product choice.

Choosing by habit rather than application

A fixing route that works well on one project may not be the right answer on another if the load case or substrate changes.

Reducing the decision to installation speed alone

Faster installation can be valuable, but it should never outweigh suitability for the actual application.

Overlooking installation control

Mechanical anchors need correct installation practice and chemical anchors depend heavily on preparation and curing discipline.

Assuming documentation is secondary

In many steel construction projects, approval route and document readiness are part of the product decision, not an afterthought.

How Fabory supports the right selection

The right support goes beyond anchor availability. It also means helping customers connect product choice to application need, documentation and project continuity.

Fabory helps customers reduce uncertainty around anchor choice, application suitability and supporting project requirements.

Fabory supports steel construction customers with more than product supply alone. The wider approach is built around helping teams choose the right fixing route for the application while keeping documentation, specification and installation context in view.

Fabory support can include:
• support for anchor selection aligned to application
• availability and dependable supply
• support for engineers, buyers and QA teams
• guidance around documentation and approval awareness
• a more complete route to steel construction project support

The aim is to help customers make more confident mechanical and chemical anchor decisions with fewer avoidable project issues.

Related topics worth exploring

Mechanical and chemical anchor selection sits alongside wider questions about anchoring, documentation and steel construction compliance.

Anchoring steel to concrete
ETA and DoP explained for anchoring systems
Certificates and documentation in steel construction
Threaded rods and studs in steel construction
HV vs HR assemblies in steel construction

Need support with mechanical or chemical anchor selection?

Talk to Fabory about anchor selection, documentation support and the right route for compliant steel construction supply.

Talk to Fabory
Sluit deze pagina niet. De melding verdwijnt zodra de pagina klaar is met laden.