text.skipToContent text.skipToNavigation
Dear visitor, currently we sometimes are showing multiple values for features on product pages. This is only an error in showing the values multiple times, the value that is showed is the right value. We apologize for this inconvenience.

Knowledge Center

      Quality & Technology
      Cadenas 3D Portal
      Technical information

         Steel
         Stainless Steel
         Surface Treatments

            Zinc or zinc alloy electroplating
            Mechanical zinc plating
            Hot dip galvanization
            Zinc flake coatings
            Anti-seize coatings

         Self Locking
         Imperial Fasteners
         Anchoring
         Conversion Tables

      Assortment
      Safety

MECHANICAL ZINC PLATING

Zinc can also be deposited on steel and other metals by means of a rotating drum filled with zinc powder, chemicals and glass balls of different diameters. When the products are introduced into this drum, the glass balls hammer the zinc onto the surface of these products, which creates a zinc layer comparable to zinc electroplating. Afterwards, the plated products are given a passivation layer, just as after the electroplating process. Mechanical zinc plating is less common for fasteners than zinc electroplating, but it has an advantage: there is no risk of hydrogen embrittlement. However, the buildup of the zinc layer must be tightly controlled in order to prevent thread interference. The mechanical plating process is standardized in ISO 12683. 


Source: Thielco Metal Coating